{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is a time delay available on the ATV312 logic inputs?
Issue:
Time delay feature on the ATV312 logic inputs

Product line:
Altivar 312, ATV312

Environment:
all

Cause:
Delay before activation

Resolution:
The Altivar 312 does not offer a delay time for the Logic inputs.  An external timer can be added if needed.

Schneider Electric Saudi Arabia