Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the ATV61/ATV71 minimum speed setting adjusted?
Issue:
Adjust minimum speed on ATV61/ATV71.

Product line:
ATV61 ATV71

Environment:
All

Cause:
Modify speed reference

Resolution:
Go to the Simply Start or Settings menu.  Find parameter Low Speed and set to the desired minimum speed reference.