Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I reset the password from the HMISTU / HMISCU when the USB media is set to use security?
Unfortunately there is no way to overwrite the security in a HMISTU or HMISCU if the USB media is set to use security.
The unit must be sent to our repair center and the application will be deleted.

Please contact Customer Service at:
Email: industrialrepair@schneider-electric.com
www.schneiderelectricrepair.com