Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is a tool to create. xrio files like a Xrio Converter For example , When we are importing these xrio files in Omicron these files are not be supported for Micom P44x relay?
Issue :
Tool to create. xrio files like a Xrio Converter for MIcom P44x relay

Product Line:
Micom P44x ,P54x

Resolution:
We have not a Xrio Converter, you need to work with the Xrio file available on Omicron site ( attached as example  )and adapted the values according your settings.

then You need to import this file in the 'Advanced Distance' module on Test Universe.

With this file, you will have your characteristic. With the export from Easergy Studio, you export all the settings but the characteristic is missing.

Schneider Electric Saudi Arabia

Attachment(s)
AREVA P441 P442 P444 E33 ENU TU2.20 V1.000.xrio [2.75 MB]