Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you set up the ATV61/ATV71 drive with an VW3A3316 ethernet IP option card to use assemblies 100 and 101?

Issue:
How do you set up the ATV61/ATV71 drive with an VW3A3316 ethernet IP option card to use assemblies 100 and 101?

Product Line:
Altivar ATV61 ATV71 with VW3A3316 or VW3A3320 option cards

Environment:
All

Cause:
Using an Allen Bradley PLC they need to set up the ATV61 with an VW3A3316 ethernet IP option card to use assemblies 100 and 101.

Resolution:

PLC settings:

The Ethernet Scanner Module needs to be configured as followed.
1.  Set up the input and output tables as a Generic option.
2.  Assembly 100 output table Size 16 bytes (8 integer) (writing command)
3.  Assembly 101 input table Size 16 bytes (8 integer) (reading command)
4.  Configuration size 0.
5.  Single INT or single Integer.

Drive settings:
[Note] - programming example only you can configure the drive to match your logic input configuration.

1.  Menu 1.6 [COMMAND]
Ref 1 channel = Com card
Profile = I/O profile
CMD Switching = LI3
CMD channel 1= Com card
CMD channel 2= Terminal control
ref 2 Switching = channel 1 active

2.  menu 1.7 [APPLICATION FUNCTION]
Ref Switching
Ref 1 B Switching = LI3
Ref 1 B channel = AI1

Programming will match LI3 to switch between Com card command and reference / Terminal command and AI1 speed reference.
Example LI3=1 Drive is commanded from terminal command and speed ref is from AI1
LI3=0 Drive is commanded from com card and speed ref is from the com card.

Using assemblies 100 and 101 will allow will the PLC's Scanner module to interface with the Drives internal Com Scanner modules in menu 1.9.

3.  Menu 1.9 [COMMUNICATION]
Set up your IP address 123 456 789 456 (example)
Set up your Subnet address 255 255 255 0 (example)
Set up your Gateway address if it applies.

Com Scanner INPUT Table is used for assembly 101 Read only
3201 ETA drives status word
8604 rFrd output speed in RPM's
0
0
0
0
0
0

Com Scanner Output table is used for assembly 100 write only
8501 CMD or command word to start the drive
8602 LFRD speed reference in RPM's
0
0
0
0
0
0
0
0
To add additional parameter addresses please refer to the ATV61/71 Communication Parameters Manual on the Schneider Electric website.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)