Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Smoke Purge option Available on ATV660 Enclosed Drives?
Issue:
​Smoke Purge option on ATV660 Enclosed Drives.

Product Line:
ATV660, Altivar 660

Environment:
All

Cause:
Smoke Purge option is not listed in Catalog

Resolution:
The Smoke Purge is available as an Engineered To Order (ETO) option for the time being.  See your local distributor or Area Drives Manger for details.

Schneider Electric Saudi Arabia

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Product Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre