Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Server error in '/reporter' Application. Login failed for user 'ION'. Reason: The password of the account has expired.
Issue:
A customer is attempting to access web reports within PME and received the error message below:

Password Expired

Product Line:
Power Monitoring Expert 7.2.2
Power Monitoring Expert 8.0
Power Monitoring Expert 8.1

Environment:
Web Applications - Web Reports

Cause:
The password for the SQL ION account has expired.

Resolution:
1) Open SQL Server Management Studio on the PME server
2) Expand the Security < Logins section
3) Right-click on the 'ION' account and select 'Properties' from the menu
4) Uncheck 'Enforce password expiration' and click 'OK'
5) Open a command prompt window and run the command 'iisreset'
6) Once the reset completes log in to the PME web page and confirm that reports can now load successfully

Schneider Electric Saudi Arabia

Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: