Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does Obr mean on Drive Status display when ramping down on ATV61 and ATV71?
Issue:
Why does my drive show Obr on display when ramping down on ATV61 or ATV71?

Product Line:
ATV61, ATV71, Altivar 61, Altivar 71

Environment:
All

Cause:
N/A

Resolution:
Obr [Overbreaking]  is a drive state and not a fault. It is displayed in the top left corner of the graphic keypad if the drive is decelerating and using the Auto-Adapted Deceleration Ramp to avoid a possible overbreaking fault (ObF). This status may show up when Decel Ramp Adapt parameter is enabled.