Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the suffix "EU" indicate on a ATV630 drive?
Issue:
"EU" suffix on a ATV630 drive

Product Line:
Altivar Process Drive

Environment:
ATV630/ATV930

Cause:
EU Suffix

Resolution:
EU indicates the drive is rated for IP55 (Nema 12) and includes a disconnect switch.