{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What remote keypads can be used with the ATV320?
Issue:
Remote keypad that is used with the Altivar 320 AC Drive.

Product Line:
ATV320 drives

Environment:
Remote keypad

Cause:
Installation

Resolution:
Several remote keypad options are available.

Option 1
VW3A1101 Graphic Display Keypad
VW3A1102 Remote Mount Bezel, IP54 (or the VW3A1105 if not being mounted)
VW3A1103 Optional Cover/Door for Bezel (increases rating to IP65)

Option 2
VW3A1111 Graphic Display Keypad
VW3A1112 Remote Mount Kit IP65
Both the ATV320 VFD and the VW3A1111 keypad firmwares have been upgraded to support compatibility. (6-2019)
Firmware versions required:
ATV320-  V2.9IE37
VW3A1111-  V2.0IE51
Earlier versions are not compatible.

Option 3
VW3A1006 Remote Terminal Keypad, IP54

Option 4
VW3A1007 Remote Terminal Keypad, IP65

Then choose one cable to connect the remote keypad to the VFD:
VW3A1104R10 1 meter
VW3A1104R30 3 meter
VW3A1104R50 5 meter
VW3A1104R100 10 meter

Schneider Electric Saudi Arabia

Attachment(s)
Cat_ATV320_keypad and options.pdf [223.14 KB]