Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to change the motor related timers of the Process Drive from seconds to minutes?

Issue:
Early versions of the ATV600 and ATV900 drives only displayed time in seconds

Product Line:
Process Drive

Environment:
All models and serial numbers

Cause:
None

Resolution:
For ATV600 series drives with firmware V2.4 and less and ATV900 V2.1 and lower, it is not possible to change the motor related timers from seconds to minutes.
For more recent versions the time is available in Days/Hours/Minutes/Seconds format.

You can view the current values and reset the timers in the Counter Management menu.

Counter management can be found in menu 4.9.
The following counters can be monitored:
[Motor Run Time] - rtH
[Power-on Time] - PtH
[Fan Operation Time] - FCPt

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team. If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)