Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
M221 Replacement Connectors

Issue:
What are the part numbers for the M221 connectors.

Product line:
TM221

Cause:
Either missing connectors or need connectors to be wired up before the system arrives for install.

Resolution:
TMAT2CSET - connector set for M221C - IO
TMAT2MSET - connector set for M221M and TM3 - IO
TMAT2MSETG - connector set for M221M and TM3 - IO Spring
TMAT2PSET - connector set for M2X1 - power supply

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)