Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What versions of the ATV32 Drive is the Profinet card compatible with?
Issue:
ATV32 Drive Profinet card

Product Line:
ATV32, Altivar 32

Environment:
All

Cause:
N/A

Resolution:
The VW3A3627 option module is compliant with Altivar 32 with versions of V1.8 IE11 or higher.