Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does COM'X 510 support RSTP?
Product Line
COM'X 5xx

Environment
Protocol support

Resolution

No, The COM'X 510 does not support RSTP.

The Rapid Spanning Tree Protocol (RSTP) IEEE 802.1W standard is available to address the Spanning Tree Protocol (STP) convergence time gap issue. Rapid Spanning Tree Protocol (RSTP) enables STP Root Ports and STP Designated Ports to change from the blocking to forwarding port state in a few seconds.

COM'X 510 only uses a single static default gateway for routing traffic It does have a Switch mode or a dual mode.
Switch mode - in which the eth1 eth2 ports work as a standard network switch and the COM'X has one IP
Dual mode - in which the ethernet 1 and ethernet 2 ports work as separate networks and the COM'X has two IP