Issue:
Process for downloading and deploying the StruxureWare Data Center Expert Virtual Appliance.
Product Line:
StruxureWare Data Center Expert (DCE)
Environment:
StruxureWare Data Center Expert Virtual Appliance (all versions)
VMware ESXi
HyperV
Resolution:
Deploying on Hyper-V HERE.
1) Download the StruxureWare Data Center Expert Virtual Appliance Trial (AP94VMTRL) from www.apc.com.
2) Once the DCE Virtual Appliance is downloaded, it can be deployed within a VMware ESXi environment. As of Version 8.1, support for HyperV has been added.
3) Information on deploying the OVF file can be found at the VMware Documentation Center.
Note: Deploying OVA shows "Invalid Certificate" on vCenter 7.0U2, but shows "Trusted certificate" in older versions. https://kb.vmware.com/s/article/84240
4) It is highly recommended to add an additional hard disk to the virtual appliance. For instructions, see knowledge base Data Center Expert | Configuring Hardware Resources (RAM, CPU, Hard Disks, & Network Adapters) .
After initial login with apcsetup, our setup prompts require the change and creation of crucial system accounts. Below are the default credentials that are required to configure new user credentials. Based on software versions, you may be prompted to change them. Please note that the apcreset password you set will be the ONLY recovery option in the event of lost or forgotten credentials.
Username: apcsetup
Password: apcsetup
Username: apcinfo
Password: apcinfo
Data Center Expert version 7.9.3 and later:
Username: apcreset
Password: apcreset
Data Center Expert version 7.9.2 and earlier:
Username: apcreset
Password: apc
Released for: Schneider Electric Saudi Arabia
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Centre
Find support resources for all your needs, in one place.