Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Cannot find the UA OPC Tools in OFS
Issue
The option to install the UA OPC tools cannot be found during the install of OFS 3.6, SP1.

Product Line
OFS

Environment
Windows 10


Resolution
The option to install the UA OPC tools cannot be found during the install of OFS 3.6, SP1.

The UA OPC Tools (UA Client, UA Configuration, UA Wrapper) were never meant to be used by the customer. The
tools were intended for development only and have been removed from OFS as of version 3.6, SP1.