This article provides details about different types of licensing available for Geo SCADA.
Ways to license Geo SCADA:
Geo SCADA may be licensed through a USB dongle or a license file. A USB dongle license is not tied to a particular machine and may be switched to a different machine if needed. A license file is specific to a particular machine it was generated for and cannot be moved to a different machine.
Types of Geo SCADA licenses:
Geo SCADA licensing makes use of a server license and a client license. A server license is needed to license a Geo SCADA server and a client license is needed to license a ViewX client. Both server and client licenses may come as USB dongles or license files.
Information about your server license is obtained from License Details.
Information about your client license is obtained from the Configure Connections dialog on the machine hosting the ViewX client.
Each server license also includes a client component to license the local ViewX client that runs on the server PC.
Floating license vs client license for ViewX:
A ViewX client is able to connect to a Geo SCADA server by using a client license that resides on the same machine as the ViewX client itself. A ViewX client may also connect to a Geo SCADA server by way of 'server side client licensing'. In the latter case, the server license must have 'x' number of client connections available to provide to ViewX clients that do not have a license of their own. This is referred to as a "floating license". The screen capture below shows an example of a Geo SCADA server license that has 2 floating ViewX licenses. This means that 2 ViewX clients (that do not use client licenses) may connect to this system by using floating licenses on the server.
A ViewX client is not able to connect to a Geo SCADA server if:
- It does not use its valid client license
- The server license does not allow for any floating ViewX clients
It is possible to configure a ViewX client to either use its own client license or a floating license on the server by enabling or disabling the "Use Client Licensing" option. If the option is enabled, the ViewX client will use its own client license to connect. If the option is disabled, the ViewX client will use a floating license if any are available on the server.
Running without a license:
Without a valid license, Geo SCADA is able to run in the Demonstration Mode. During the Demonstration Mode, the system is limited to:
- 2 hours of runtime before the Geo SCADA server automatically shuts down
- Server redundancy is disabled
- Point count is limited to 1000 points
- Keep the Enable 100-Point Indefinite Demo License check box clear.
- If the Enable 100-Point Indefinite Demo License box is checked, then you can run 100-point indefinite demo license but it restricts the ViewX license to be Local ViewX only.
Please note that Geo SCADA will switch to the demonstration Mode even when a valid license is being used if:
- The number of points allowed by the license is exceeded
- An unlicensed driver is being run
When in the Demonstration Mode, an alarm will be raised to indicate that the license will expire in under 2 hours. When only fifteen minutes is left before the Demonstration Mode is finished, another alarm will be raised to indicate this.
Released for: Schneider Electric Saudi Arabia