Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What's the difference between reference XVUC29 and reference XVUC29P?
There are following differences:
1. XVUC29 is driven by ON/OFF signal and usually connect to relay, XVUC29P is driven by pulse signal and usually connect to PTO/PWM or transistor.
2. XVUC29 only can be changed color and mode by dip-switch, XVUC29P can be changed color and mode by input pulse signal.
3. XVUC29 supports maximum 5 layers, XVUC29P supports maximum 4 layers.
4. XVUC29 can be assembled in any layer, XVUC29P only can use under single color light unit.