Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the sheet metal thickness for Prisma iPM System M?
For Prisma iPM system M, the sheet metal thicknesses are as follows:
  • Framework --> 2 mm
  • Rear panels --> - 1.5mm
  • Side panels --> 1 mm
  • Roof --> 2 mm
  • Bottom panels --> 1.5 mm
  • Front plates --> 1 mm
  • Door --> 1.5 mm