Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Ethernet communication protocols are available for M221 controllers with an Ethernet port?
TM221CE*** and TM221ME*** controllers have an embedded RJ 45 Ethernet port (10/100 Mbps, MDI/MDIX) with Modbus TCP (Client/Server), EtherNet/IP (adapter), UDP, TCP protocols.