Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum available current on ATV12 Drive 24Vdc Power Supply?
Issue:
Maximum available current on ATV12 Drive 24Vdc Power Supply

Product Line:
ATV12, Altivar 12

Environment:
All

Cause:
N/A

Resolution:
Maximum customer current available is 100 mA (+ 24 VDC -15% +20% protected against short-circuits and overloads).