Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
TM251MESE : Modbus TCP IOscanner channel status can be wrong
With TM251MESE firmware v4.0.4.14, when using Modbus TCP IO scanner with more than 16 channels, channels health bits may be wrong.

Firmware v4.0.5.10 (available with SoMachine v4.2) solves this issue.