Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many Modbus RTU server devices can be connected to an HMIGTO
Issue:
Looking for specifications on how many Modbus RTU server devices can be connected to an HMIGTO

Product LIne:
Harmony, Mageils, HMIGTO, HMIGTU, HMISTU, XBTGT, XBTGK, HMIGK

Resolution:
The maximum number of Modbus RTU server devices that can be connected to a Magelis HMIGTO is 32.

The RS-485 communication cable has to be shielded and terminated properly and the maximum distance between devices is 100ft.