Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for braking resistors for the ATV600 series drives?

Issue:
Customer wants to add a braking resistor to the ATV600 series drive.

Product line:
Altivar Process, ATV630, ATV660, ATV650, ATV680

Resolution:
The ATV600 series Process drive does not have the DC bus connections, PA and PB, to add a brake unit/resistor.  The target application for this product line is pumps and fans, which normally do not need the brake function.
If the application has high inertia, try increasing DEC time or change to freewheel stop mode.
If a low DEC is required and dynamic braking is needed to prevent OBF or SOF faulting, then consider using the ATV900 series VFDs.

***

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions: Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance: Support | Schneider Electric Global (se.com)