Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
MiCOM relays. Is it possible to send and activate cid/mcl configuration via ethernet?
Starting from Easergy Studio V7.0.0 it is possible to send IEC 61850 configuration file (.mcl or .cid) via ethernet connection. It is also possible to switch data banks.

It is not possible to send configuration directly from the IED Configurator via ethernet connection.

Mentioned above functionality is available for Px4 and Px3 relays only.