Issue:
ATV320 single phase supply to a three phase motor
Product Line:
ATV320, Altivar 320 Machine drive
Environment:
All models
Cause:
Short circuit and HP ratings for VFDs supplied with single phase power.
Resolution:
Yes, the ATV320 is suitable for single phase supply to three phase motors. See the information included in the Getting Started Annex, document NVE21777 attached to select.
ATV320 single phase supply to a three phase motor
Product Line:
ATV320, Altivar 320 Machine drive
Environment:
All models
Cause:
Short circuit and HP ratings for VFDs supplied with single phase power.
Resolution:
Yes, the ATV320 is suitable for single phase supply to three phase motors. See the information included in the Getting Started Annex, document NVE21777 attached to select.
Released for:Schneider Electric Saudi Arabia