Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
I changed my IP configuration of IFE to DHCP through Ecoreach, but the device value shows static. What could be wrong here?
Once you change the IP configuration to DHCP and transfer the settings to the device,  the device gets disconnected and hence shows the earlier value. If the Ecoreach device home page shows the device is still connected, please disconnect and connect again with the right IP address entered in connection parameter.