Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why doesn't Vijeo Designer show which objects have errors?
Issue:
When building a Vijeo Designer project, it shows the error "build has aborted, 100 Errors." in the feedback zone.

Product Line:
Vijeo Designer (all versions)

Resolution:
In Vijeo Designer, it is possible for the Feedback zone to not show what objects have errors when there are more than 100 errors. In one specific situation, you will only be informed of 100 errors without any other details. In this case, check if you have any invalid text resources. If you do, either correct the text resource or delete it completely.