Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the frame sizes for the Altivar 650 and 950 Process drive?
Issue:
What Frame sizes are available for the Altivar 650 and Altivar 950 Process drive.

Product Line:
Altivar Process Drive (ATV650, ATV950)

Environment:
All serial numbers for Altivar 650 and Altivar 950

Cause:
N/A

Resolution:
The ATV650 drives are a version of the Altivar Process open drive (IP21) with a more robust housing for higher protection (IP55).
They come in 3 different Frame sizes described below.

Size A
  • 400/480Vac
    • Includes the ATV630 and ATV930 from frame sizes 1 to 3
    • 0.75 – 22kW (1 - 30hp)
    • ATV650U07N4, ATV650U15N4, ATV650U22N4, ATV650U30N4, ATV650U40N4, ATV650U55N4, ATV650U75N4,
      ATV650D11N4, ATV650D15N4, ATV650D18N4, ATV650D22N4
Size B
  • 400/480Vac
    • Includes the ATV630 and ATV930 frame size 4
    • 30 – 45kW (40 - 60hp)
    • ATV650D30N4, ATV650D37N4, ATV650D45N4,
Size C
  • 400/480Vac
    • Includes the ATV630 and ATV930 frame size 5
    • 55 – 90kW (60 - 125hp)
    • ATV650D55N4, ATV650D75N4, ATV650D90N4
ATV650 and ATV950 Frame Sizes