Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I change the color of an image from the toolchest in Vijeo Designer?
Issue:
Looking for a way to change the colors of an image from the Toolchest of Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
The images from the Toolchest are static and cannot be modified within Vijeo Designer. However, you could copy the image to a JPG or PNG file and modify it in a Graphical Editor like Adobe Photoshop or MS Paint.