How to know the OFS SP version installed on my PC?
There is a version of reference, OFS 3.50, and this version has an internal code, OFS V3.50 _ InternalCode
After that each time an SP is created value to this internal code is incremented by 1. Only the OFS device (client, server, configuration tool…) impacted by the evolution, reports the new internal number linked to the SP.
So better way to know the version used is to check this via the Control pannel
Information between the SP number and this internal code can be found inside the file content.html that it is on the OFS CD.
After that each time an SP is created value to this internal code is incremented by 1. Only the OFS device (client, server, configuration tool…) impacted by the evolution, reports the new internal number linked to the SP.
So better way to know the version used is to check this via the Control pannel
Information between the SP number and this internal code can be found inside the file content.html that it is on the OFS CD.
Released for: Schneider Electric Saudi Arabia