Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of read_var and write_var that I can call simultaneously?
Issue:
Maximum number of function blocks read_var and write_var simultaneously in SoMachine

Product Line:
SoMachine

Resolution:
Maximum number of simultaneous READ_VAR and WRITE_VAR blocks is 8 (because 8 TCP connections).