Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the M580 have system words indicating IO module health?

Issue:

Does the M580 have system words indicating IO module health?

Product Line:

M580, Control Expert

Resolution:

Yes, system words %SW160 to %SW167 indicate IO module health.
These words detect errors for racks 0 through 7.

System words %SW160 to %SW167 are associated, respectively, to racks 0 to 7.

Bits 0 to 15 of each of these words are associated with the modules located in positions 0 to 15 of these racks.

The bit is at 0 if the module has a detected error, and at 1 if the module is operating correctly.
Example: %SW163.5 = 0, the module located in position 5 on rack 3 has a detected error.

In case of half racks, 2 contiguous half racks make a complete normal rack, referenced by only one %SWi.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)