Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the Closing conditions for the MN release coil inside NSX MCCB ?

If there is no supply to the MN release, it is impossible to close the circuit breaker,

either manually or electrically. Closing is ensured when the voltage supply to the

release U u 0.85 x Un. Below this threshold, closing is not guaranteed.