Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does Schneider-Electric have a regenerated VFD that will return back the voltage to the line?
Issue:
Schneider-Electric return back the voltage to the line.

Product Line:
ATV930

Environment:
Regen drives

Cause:
Product Selection

Resolution:
1) ATV980 is a series of regenerative drives:
https://www.se.com/ww/en/product-range/63124-altivar-process-atv900/914058402-drive-systems?N=201182946&Nr=AND(P_visibility:1,product.siteId:700002,OR(product.catalogId:catalog50001))&Nrpp=10&parent-subcategory-id=86129#tabs

2) There are Altivar Regenerative Units : ATVRU75N4, ATVRD15N4 - they can evacuate energy back to the supply lines.
They can work with ATV320/340, ATV6xx/9xx, drives.
https://www.se.com/ww/en/product/ATVRD15N4/regenerative-unit---15-kw---for-altivar-variable-speed-drive#search?langType=englishUTF8
https://www.se.com/ww/en/product/ATVRU75N4/regenerative-unit---7,5-kw---for-altivar-variable-speed-drive#search?langType=englishUTF8
https://www.se.com/ww/en/download/document/NVE88423/
https://www.se.com/ww/en/download/document/NVE94856/

3) For ATV71 use Altivar AFE (Active Front END)
https://www.se.com/ww/en/product-range/7555-altivar-afe-(active-front-end)?N=3936592704&parent-category-id=2900&filter=business-1-industrial-automation-and-control