Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the temperature limit conditions for the Altivar Process Drive (IP55)?
Issue:
Temperature conditions for the Altivar Process Drives

Product Line:
Altivar 650 and Altivar 950 (IP55)

Environment:
All serial numbers for Altivar 650 and Altivar 950

Cause:
N/A

Resolution:
All IP55 Products, Drive Systems and Floor Standing Products can be operated up to 40°C without de-rating and up to 50°C with de-rating.
The de-rating factor depends on the ambient temperature, the mounting position and the switching frequency (see installation manual).