Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the GT500-480 Door Switch?
Issue:
A customer would like to know the part number and specifications for the GT500-480 door switch.

Product Line:
GT500-480, GT500-600

Environment:
Installations that utilize the GT500 series inverter

Cause:
A product description and confirmation of part number is required when creating a case for a parts order.

Resolution:
The APC Part Number is 531-2017-01.
The specifications can be found below in the attachment.

Schneider Electric Saudi Arabia

Attachment(s)
062-2017-01_SE.pdf [1.63 MB]