Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many expansion slots can be installed on the Altivar Process Drives?

Resolution:
The Altivar 600/900 Process has 2 expansion slots:

  • Slot A (Right)
    • Legacy communication options
    • Advance Ethernet (only for ATV600)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
  • Slot B (Left)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
    • Encoder Module (only for ATV900)
  • Slot C (Top) - (VW3A3800 - Only for ATV900)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
    • Safety option “premium” (VW3A3802)


Control electronic size does not change (even with 2 expansion cards used).
It is not possible to use the same expansion card twice and maximum one communication card is allowed.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)