Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the ATV630 Modbus port have a built-in Terminating resistor?

Issue:
ATV630 Modbus port built-in Terminating resistor

Product Line:
ATV630, Altivar 630, Process Drive

Environment:
All

Cause:
NA

Resolution:
No, the resistor has to be installed externally.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)