Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to send the status of VIP410 watchdog via Modbus communication?
Unfortunately, for VIP410 relay, it is not possible to send the status of the watchdog via Modbus communication. There is no available Modbus address for the watchdog function.