How can we help you today?

How many Sepam measurement can MSA141 module convert into analog signal?

Issue

A user wants to know how many Sepam measurements or parameters can be converted into an analog signal using the MSA141 module.

Product

  • Sepam MSA141 Module
  • Sepam Protection Relays

Environment

  • Analog Signal Conversion
  • Monitoring Systems
  • Industrial Automation
  • Protection Relay Applications

Cause

When integrating Sepam relays with analog monitoring, control, or SCADA systems, users may need to determine the number of Sepam measurements that can be mapped to analog outputs through the MSA141 module.

Resolution

The MSA141 module can convert only one Sepam measurement or parameter into an analog signal. If multiple measurements need to be converted to analog signals, additional solutions or modules must be considered, as a single MSA141 module supports only one analog output value at a time.

Schneider Electric Saudi Arabia