Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the largest SD card we can use for the HMIG3U?
Issue:
What are the specifications of the largest SD card we can use with the Magelis HMIGTO and HMIG3U?

Product Line:
HMIG3U, HMIGTO series

Resolution:
The largest SD card that can be used with the HMIGTO and HMIG3U is 32GB formatted as FAT32.