Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use one large line reactor on multiple drives vs one line reactor for one drive?
Issue:
Is it possible to use one large line reactor on multiple drives vs one line reactor for one drive?

Product Line:
Altivar Drives

Environment:
All

Cause:
Would like to use only one line reactor and feed multiple drives.

Resolution:
No, it is best to have individual line reactors. If a single line reactor is used, it will have lower inductance and may not be enough if a single drive is running.