{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM5560 mailbox registers
The mailbox registers (5580 -5679) are used to store any user data values within UINT16 (0-65335) size by write command through Modbus application.The written user data values can be readable by using the same registers.Any Modbus application can be used for this read and write function.

So basically those registers are for keeping and referring any downstream meters values by writing in this registers.

Schneider Electric Saudi Arabia

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.