Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What should the F601 current limit parameter be set to in the ATV212 drives?
Issue:
ATV212 parameter F601 configuration

Product Line:
ATV212, S-Flex 212

Environment:
All

Cause:
What should the F601 current limit parameter be set to in the ATV212 drives?

Resolution:
The F601 Current limit parameter should be set to 110% of the Drives current rating.
Note: If you use a small size motor on a larger drive, you will need to adjust this setting to the motor FLA times 1.1.