Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find electrical control drawings for the ATV660 and ATV960 enclosed drives?

Issue:
Electrical control drawings for the ATV660 and ATV960 enclosed drives.

Product Line:
ATV660 and ATV960 drives

Environment:
all

Cause:
Needs to get electrical drawings for the ATV660 drives.

Resolution:
The drawings are no longer in the back of the manual like the E-flex drives
Drawings for the ATV660 and ATV960 will only show up after you have submitted your order in Q2C.
You will need to contact the Drives Product Support Group or the Project Manager with the factory order number.