Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does the BRH parameter mean in Somove?
Issue:
BRH parameter meaning in Somove.

Product Line:
ATV71 drives

Environment:
All

Cause:
BRH appears in the Somove software but does not show up in the drives parameters.

Resolution:
BRH on somove is the setting word of BRHB0, BFRHB1, BRHB3, with for example BRHB0=1 and BRH3=1 the, BRH=5.