{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the prerequisites for Ecostruxure power commission?
PC Hardware requirements
ComponentMinimum Requirements
ProcessorIntel Core 2 Duo CPU at 3.00 G Hz
RAM4GB
System Type64 bit or 32 bit
Software Requirements
Microsoft Windows® 10 operating system with. net framework 4.8 support.

NOTE: Windows10 versions 1507 and 1511 do not support.net framework 4.8.

•Modbus driver (version2.20 IE 30for32-bit an dversion3.20 IE30 for 64-bit )

•Require atleast 2GB free space in the drive where EcoStruxure Power Commission will be installed.
NOTE: Make sure to follow the below guidelines before starting the installation.

NOTE: Make sure to follow the below guidelines before starting the installation.

•User should have access to
RunNode.exe
User should have full permission to:
◦%UserProfile%\Documents\Schneider-Electric\Ecoreach
◦%UserProfile%\AppData\Roaming\Schneider-Electric\Ecoreach
◦%ProgramData%\Schneider-Electric\Ecoreach


Register
To log in, first time or to register for Ecoreach access to the internet is required.

Internet Connection
Internet connection is required to do the Ecoreach Registration after installation.
Ecoreach can be connected to the internet over a Wi-Fi connection or 3G/4G/5G dongle.


Schneider Electric Saudi Arabia

Attachment(s)
Ecoreach_V2_5_Installation_Guide.pdf [1.21 MB]
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.