Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is conformal coating available with the Altivar 320 drive?
Issue:
Is conformal coating available with the ATV320?

Product Line:
Altivar 320 Drives

Environment:
All serial numbers for Altivar 320 Drives

Cause:
N/A

Resolution:
Yes, the Altivar 320 come with conformal coating for increased robustness against polluted atmosphere.