Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Fan PID function on the Altivar 600 Process Drive?
Issue:
Altivar 600 Fan PID function.

Product Line:
Altivar 600 Process Drive

Environment:
All products of Altivar 600 Process Drive

Cause:
N/A

Resolution:
The Fan PID allows the user to setup a basic PID function when the drive's Macro Configuration (Menu 7.1) is set to Generic Fan Control.
There is no difference in the parameters and the settings than when setting up a pump PID.
To access go to [Fan] - [PID controller]